How to plot in radian scale (instead of Hz) in ac analysis
I assume you meant radian per second (rad/s), where Omega=2*PI*Frequency.
In .AC, .qraw with .alias Freq=Frequency and Omega=(2*PI*Frequency), so change the x-axis quantity to Omega.
Well, the number itself correctly follows Omega, but it still displays Hz as the unit. I will report this to Mike for his review. Currently, you can use Omega/1Hz to remove the unit display.
- Update Qspice: the alias of Omega is changed to (
2*PI*Frequency*1s) in .qraw, indicating that plotting Omega will no longer display a unit in Hz. - To work with Omega, you may still want the x-axis log scale to begin and end with 10 times. My recommendation is to do a trick at start and stop frequency by dividing it with
/2/PI. - If the auto-zoom x-axis not fully fitting is bothering you, consider submitting it to Mike for review through email.
ac radian.qsch (4.3 KB)
Update to the latest version of Qspice, and now you can directly plot a Bode plot with the x-axis as Omega using the .abscissa command.
03/20/2026 Implemented a .abscissa command to configure a default parametric plot.
ac radian (.abscissa).qsch (4.3 KB)