QSPICE SI Simulation: Problems Encountered

Hi everyone,

I’m working on a small USB 3.0 Gen1 (5 Gbps) 4-port hub board and trying to use QSPICE for line-level signal-integrity checks. I’m still learning, so I’d really appreciate advice from people with more experience.

The board is a 4-layer JLC3313 stackup:

  • L1: 35 µm copper

  • L1–L2 prepreg: 99.4 µm, εr ≈ 4.1

  • L2: 15.2 µm copper

  • L2–L3 core: 1.265 mm, εr ≈ 4.6

  • L3: 15.2 µm copper

  • L3–L4 prepreg: 99.4 µm, εr ≈ 4.1

  • L4: 35 µm copper

The two SuperSpeed pairs I’m looking at are:

  • SSRX: 0.19 mm width, 0.15 mm gap, 18.565 mm long

  • SSTX: 0.19 mm width, 0.15 mm gap, 12.954 mm long

Both are on the top layer, referenced to L2. Calculated differential impedance is about 90.7 Ω.

What I did

  1. Exported the board as ODB++ and imported it into Ansys Electronics Desktop / SIwave via PyEDB.

  2. Extracted the actual trace width, gap, length, layer, and stackup.

  3. Converted the line to a QSPICE lossy transmission line:


O1 txp 0 rxp 0 LSSRX

O2 txn 0 rxn 0 LSSRX

.model LSSRX LTRA(R=200 L=2.67e-7 C=1.3e-10 G=0 LEN=0.018565)

  1. Drove it with a behavioral GPIO-like source: 45.35 Ω per side (90.7 Ω differential), 5 Gbps PRBS7, 20 ps edges, 50 Ω receiver termination.

  2. Folded the output in Python to make an eye diagram.

The line-level eye looks open: about 0.96 V differential eye height for SSRX and 0.97 V for SSTX with a 1 V differential source. But this is still a very idealized result.

Problems I ran into

1. QSPICE lossy line does not accept nonzero G

QSPICE reports:


Nonzero G (except RG) line not supported yet

So I had to set G=0, which means dielectric loss is not included. Is there a recommended way to include dielectric loss in QSPICE, or is a different lossy-line formulation preferred?

2. Driver and receiver models

There is no public IBIS/IBIS-AMI model for the CH634X hub. As a reference I downloaded the TUSB8041RGC.ibs USB3 hub IBIS model and looked at its usb3_DE / usb3_WODE output models. It uses Rref = 50, C_comp ≈ 0.53 pF, and a ramp of roughly 15 ps.

But QSPICE does not directly consume IBIS/IBIS-AMI. What is the recommended flow?

  • Extract the IBIS ramp/V-I/C_comp into a behavioral SPICE driver?

  • Use SPISim or ADS to generate a SPICE/IBIS-AMI model?

  • Or is there a public USB3 Gen1 TX/RX model that is known to work well in QSPICE?

3. Differential pair and crosstalk

I modeled the two conductors as two independent LTRA lines. That is fine for a first eye estimate, but it does not include:

  • coupling between P and N;

  • NEXT/FEXT from neighboring pairs;

  • connector fanout;

  • package parasitics.

Is there a recommended coupled-line or crosstalk modeling approach in QSPICE? Should I use mutual inductance K, a coupled transmission line model, or a different tool for this part?

4. AC coupling and common mode

The SSTX pair has 100 nF AC-coupling capacitors. In a 111 ns transient, the 100 nF capacitors do not charge (RC ≈ 5 µs), so the common-mode operating point is not established. I had to short the capacitors for the eye simulation and treat the low-frequency behavior separately.

What is the recommended way to handle AC-coupled links in QSPICE? Should I:

  • pre-charge the capacitors with .ic;

  • add a common-mode bias network;

  • run a much longer transient;

  • or use a different termination/initial-condition strategy?

5. 50 Ω vs 45 Ω

I initially used 50 Ω source and receiver resistors, then realized that is 100 Ω differential, not 90 Ω. I changed them to 45.35 Ω per side.

Is that the correct interpretation for a 90 Ω differential line? And when using 50 Ω lab equipment, what is the recommended renormalization/de-embedding practice?

6. Connector and protection models

I don’t have good models for:

  • the USB3 Type-A / Type-C connector;

  • the AC-coupling capacitor pads;

  • the ESD protection diodes.

Do you have recommendations for PROT / ESD protection models for USB3 SuperSpeed lines, preferably low-capacitance diodes with SPICE models? And are there public connector S-parameter or IBIS models that are accurate enough for 5 Gbps?

7. Eye diagram methodology

QSPICE has no native eye-diagram feature, so I fold the waveform in Python. Is that the common practice, or is there a preferred .abscissa / measurement flow in QSPICE for eye diagrams and masks?

My main question

Is QSPICE a reasonable tool for this kind of 5 Gbps line-level SI work, or would you recommend using it only for first-order checks and moving to ADS/HFSS/SIwave for the final channel?

I’m not trying to claim compliance from this model; I’m trying to build a reliable, checkable workflow. Any recommendations for driver/receiver models, connector models, protection models, or a better QSPICE testbench would be very welcome.

Thank you for your time.

Shorting the 100 nF SSTX caps for the eye is reasonable for a first high-frequency check, but don’t use that run to judge common-mode or low-frequency droop. Run a separate, much longer transient (or set the cap initial condition/DC bias) so the AC-coupling node settles, and keep the shorted-cap eye as the high-pass-only result. For the LTRA G=0 limitation, treat the line as a placeholder and compare against an S-parameter or lumped RLGC model before trusting dielectric loss; QSPICE’s ideal LTRA eye won’t capture that.

1 Like

Thanks a lot for the detailed reply — both points are well taken. You’re right that the shorted 100 nF cap eye is only a high-frequency sanity check; I won’t use it to judge common-mode or low-frequency droop. I’ll split it into a shorted-cap fast eye plus a separate, much longer transient with proper cap initial conditions / DC bias so the AC-coupling node settles. I also agree on the LTRA G=0 limitation: it is only a placeholder, and dielectric loss should be validated against an S-parameter or lumped RLGC model. We have now shifted the main simulation effort to Ansys HFSS/SIwave S-parameter extraction and native QuickEye/MATLAB BER, so QSPICE is only used for quick time-domain checks. Thanks again for catching both issues.