Qspice Installation

Can we install Qspice on the offline computer/without internet?
Thanks

You can install as a user on 1 pc thats connected to network.

Then copy the whole Qspice folder to the offline PC… It should do the trick

Thanks you, It works.

Correct!

Note 1: This only works for user-mode installations, to my knowledge, but is an acceptable workaround. Note 2: There is a timer in QSPICE which requires a network connection every 60 or 90 days (can’t recall which); once the pace of updates to QSPICE has slowed, this timer will be removed.

1 Like