QSPICE Forum Schematic Capture "A Frequency Response Analyzer (FRA) in QSPICE"

For this week’s QSPICE schematic capture, we have “A Frequency Response Analyzer (FRA) in QSPICE” by our friend Kelvin Leung. This schematic capture is a demonstration of an in-depth project Kelvin has created using the Ø-Device (DLL-block). The FRA is a method that analyzes the relationship between signals in a system by injecting a perturbing source. (Schematic Capture Post #036) To access the project files, please go to: https://github.com/KSKelvin-Github/Qspice/tree/main/Projects/FRA%20Frequency%20Response%20Analyzer
example1.Buck-FRAnalyzerKSK.qsch (13.0 KB)
franalyzerksk.cpp (17.8 KB)
franalyzerksk.dll (61.0 KB)
FRAnalyzerKSK.qsym (4.0 KB)


Qspice Project - Frequency Response Analyzer by KSKelvin.pdf (641.9 KB)

7 Likes

This is a variant with 2 transfer functions from the FRA Frequency Response Analyzer project. Symbols, code, and examples can be found at this link:
Qspice/Projects/FRA Frequency Response Analyzer - Dual · KSKelvin-Github/Qspice

example6.TransferFunction-FRAanlyzer2KSK.qsch
Two linear transfer functions in series to demonstrate obtaining two transfer functions with a single FRA

example1.Buck-FRAnalyzer2KSK.qsch
One simulation to obtain V(out)/V(duty) and I(L1)/V(duty) transfer functions

1 Like

That’s nice upgrade…So quick! :grin:

1 Like