QPL9065 1.1GHZ~1.65GHZ Reference Design

目前器件手册中只有典型的1.7-2.7GHz、700-1000MHz、2.7~3.7GHz。目前我需要1.1GHZ~1.65GHZ的频带,请问能否提供针对该频点的更具体的设计指南,尤其是输入和输出匹配网络中的电容、电感值

Hi, unfortunately there is not an existing reference design for the QPL9065 covering 1.1-1.65GHz. If you need further support tuning the QPL9065 over 1.1-1.65GHz please contact appsupport@Qorvo.com stating your company name and location. Details of your project would be useful, as well as specifying the parameters you need to meet like gain, input and output return loss, NF and OIP3. Thanks.

您好,克里斯
增益、输入输出回波损耗、噪声系数和输出三阶交调点这些参数按芯片的实现的范围就可以
1.能否通过仿真工具提供频率1.1~1.65GHz的外围电路的电阻电容的参数设计、以及预留方案。
2.如果不方便进行仿真,能否提供该芯片的仿真模型。
ADS模型 (.zap 文件)
AWR模型 (.emp 文件)
3.手册中对700-1000MHz频率设计 C9应该是电容值,却标成了电阻值0欧姆 ,能否给出正确值。
此致,敬意

To get further support on this please contact appsupport@Qorvo.com.
Thanks.