Hi, I recently purchased QPC8019Q product, a 2-output switch. After analyzing the data sheet and the parameters of its behavior, I can only see its RF operation when you power the switch and choose the output. My question is, what happens when the switch is not powered? What response would I see on both outputs? How does the switch behave in this RF situation? I only don’t power the switch but if I inject RF into the input, can I consider it to work as open on both outputs? Or how?
I am using this device in a multi-state antenna, and when the switch is not powered (VDD = 0 and Vctrl = 0, following the datasheet recommendations not to apply Vctrl without VDD), I observe an RF response in this condition that I cannot predict, but it does affect the overall performance of my system.