Hello,
I just started to work with QM33120W, and tried to connect it via QorvoOne app.
No matter how long I waited, nothing showed up. I am using Mac(mac OS 14.5)
This is what I have checked.
-
I installed Qorvo Nearby Interaction using the application on iphone. I could detect
nRF52840DK(B17180F1) and measure the distance, angle and stuff. So I have confirmed that the board is powered and the firm ware was there and it can transmit and receive signals .The board was powered and I made sure to reset it before connecting to it. -
When I checked my usb ports, nothing showed up. I am considering that this is due to not recognizing devices by usb ports on my mac rather than the board problem.
Can someone kindly suggest any help? It will be a great honor for me.
Best,
Rieh Yu