Hello,
We are evaluating the QM35825 as a receiver and need it to receive existing
DW1000-based devices. Two Qorvo sources contradict each other on whether
this is possible.
QM35825 Production Data Sheet Rev. D (Sep 2025), §10.5:
“Packet configuration SP0 is a standard IEEE 802.15.4-2015 UWB packet
structure. This ensures backward compatibility with Qorvo’s DW1000 chip.”
But per Frame type SP0 error, the shipped
firmware reports SP0: Not supported in get_cap, and setting it returns
ErrorInvalidRFrameConfig.
Three questions:
-
Is SP0 receive missing from the firmware only, or from the silicon as
well? -
Is there any mode — PCTT, Radar, or proprietary — where the QM35825 can
receive an SP0 frame from a DW1000 and report timestamps, CIR or AoA
diagnostics? -
QORVO_FIRA_RANGE_DIAGNOSTICS_NTFencodes CIR per segment (IPATOV
included) with a primary/secondary receiver indicator. In dual RX mode,
does the device produce two IPATOV CIRs, one per receiver? If it does,
PDoA would be derivable from the preamble alone, with no STS involved —
is that available in any mode?
We have to select the transmitter-side radio before the next board
revision, so a clear answer either way is what we need.
Thanks.