I purchased the QM33120WDK1 from mouser and the board doesn’t connect to PC over USB connector(J3) on nRF52840DK.
I only see D1,D2 LED blinks for a second but PC doesn’t even detect the USB connection. As per quick user guide, there is no instruction other than connecting USB and running QorvoOne.
I am using Windows 11 Pro
Just FYI, JLink Debug Connector(J2) seems to atleast show up in device manager.
I have the same problem with this Kit. Also from Mouser.
QorvoOne is not detecting any devices conected throught USB.
I also see leds flashing for a second…
I’m using Iwndows 10 Pro.
How to solve this?
Thank you
Hi, I have come across the same problem.
But when I try to flash SDK Firmware by using JFlashLite, it shows that no probes are connected via USB. How can I solve the problem?
You need to plug in your board by using the J2 connector in the picture above. After the flashing is done, you can use the J3 connector to communicate with the QM33.
Hi @Sending, can you please post the serial numbers of your boards. They are on the sticker on the red boards and should be in the format Q1yywwxxxx and Q2yywwxxxx. We want to figure out why/how they have been shipped without firmware. Thank you.