Hi all, great simulator and schematic entry, I love it.
Found a snag with PWL source in a subct., it gives a syntax error and the run button stays red forever. See pics:
I’m also facing this bug which prevent me from creating my dream workspace
What I would like to create is
parameters in a “parameters” folder (with multiple txt files externally generated from an Excel table)
sub-circuits also defined in a dedicated folder
main schematic at the root of those folders
Currently, I’m stuck with tens of PWL generators in the main file, and it looks ugly.
The objective of such workspace would be to make complex systems easier to understand. With a nice high level schematic (which also could be used as a grounding schematic), and multiple sub-circuits which would enable the user to dig into smaller parts of the system.