Hi, I just received 5 DWM1001 DEVELOPMENT BOARDS and I want to test it with Decawave DRTLS Manager. I created my network, added 4 anchors and one tag, but have problems with auto positioning - I see all anchors in network details (some with very low signal), but in auto positioning menu I see only some of them, randomly. Some times I can see all anchors, but auto positioning fails with errors. Anchors are in range of 6-7 meters each other, my samsung S6 is close tho them. What is wrong and how to fix it?
How far apart are the anchors? How far away is your tablet, it needs to be within the range of all of the anchors you want to auto-position.
Your tablet/phone battery seems low (4%).
If auto-positioning fails, possibly the anchors are too far apart. Try moving them closer together (e.g. 5m apart) to get the feature working/get comfortable using the feature. And then extend the system.
Anchors are about 6 meters apart, it is not too much for BT in room. Battery is not the problem - fully loaded doesnt work better.
I set distances manually, but now I have problems to see tag on my smartphone - it appears from time to time, not too often
I think that some device is broken, but I have only five to test… Maybe it is the problem with application?