Hello,
I’m using the PAC5524AEVK1 and the pac55xx_peripheral_example code provided by qorvo.
I am running the TEST_TIMER_PWM_SYMMETRIC test. I also tried the asymmetric code.
Upon turning on the board with voltages between 20-30V, the power supply detects a short and turns off.
If the PWM is shut down, then no shorts are present, and the board works properly.
I have nothing connected to the motor terminals. I’m afraid that if I connect a motor, I might damage the board.
I have attached pictures of the UH and UL pins from the oscilloscope.
Thank you.