Good morning,
I am trying to implement the solution of using raspberry to deploy a system as per the Gateway Quick Deployment Guide. To implement this we have used a raspberry pi3 model B+ that as we had read to make it suitable it was necessary to disable the ethernet.
We disabled the ethernet and followed the guide step by step, but when we opened the web-manager graphical interface we saw that it did not see the presence of either anchors or tags even though these were powered and inserted in the same PanId, we also checked the correct setting of the configuration of anchors and tags and everything seems correct (PanId, functional modes: anchor, tag, initiator).
Looking on the forum we noticed that it might be useful to check the daemon logs.
The following information is attached:
1- linux kernel version
2- dwm-daemon logs
3- configuration file
Linux version 4.14.50-v7+ (dc4@dc4-XPS13-9333) (gcc version 4.9.3 (crosstool-NG crosstool-ng-1.22.0-88-g8460611)) #1122 SMP Tue Jun 19 12:26:26 BST 2018
Fri 25 Mar 09:50:44 UTC 2022
Starting daemon dwm-daemon with command ‘/usr/local/bin/dwm-daemon’ and options ‘-c /etc/dwm1001/dwm1001.config -l /var/log/dwm-daemon.log’…
2022-03-25 09:50:45.043 INFO [438] [leaps::core::run@60] starting…
2022-03-25 09:50:45.072 ERROR [438] [leaps::io::dev::read@100] Value missing in configuration file.
2022-03-25 09:50:50.075 ERROR [438] [main@208] Invalid function arguments provided.