Post compiling never happens

I’m confronted to a situation where the simulation works, the waves are well displayed, everything seems to have worked properly but the .meas operations never happen. I see the message "post processing compiling step 0 of11 " displayed. Then nothing happens and when I click again anywhere the message disappears but there is nothing in the tab “post processing”. Out of curiosity, i rebuilt exactly the same simulation in LTspice and there i got my measurements. Frustrating. What options do I have to test in QSPICE, to try to force these measurements? Thanks a lot

Upload your schematic. It might be a bug, but just a description alone may not provide enough information to help. Alternatively, you can report the bug to Mike via email (Qspice > Help > About) if you are certain it is a bug.

Thanks a lot . I begin to be familiar with QSPICE. After I wrote this question, I just suddenly thought to erase all instructions that won’t be executed, and to rewrite them. And now suddenly it worked. As efficient and fast as it can be ,QSPICE seems to be be sometimes a little “grumpy” in apparence. I learned again something: if you think that your simulation works, and that it doesn’t , rewrite the instructions clearly , and start on a clean slate. have a nice day. .

1 Like