PLL LOCKING ERROR CONFIG FAILED in twr_initiator

I am using dwm3000 arduino shield with eps32s3 and I used the Makerfabs-ESP32-UWB-DW3000-main code as ex_06a_ss_twr_initiator. When I upload code into board I got following error.

ESP-ROM:esp32s3-20210327

Build:Mar 27 2021

rst:0x1 (POWERON),boot:0x8 (SPI_FAST_FLASH_BOOT)

SPIWP:0xee

mode:DIO, clock div:1

load:0x3fce2820,len:0x116c

load:0x403c8700,len:0xc2c

load:0x403cb700,len:0x3108

entry 0x403c88b8

SS TWR INIT v1.0

DEVICE ID: deca0302

PLL LOCKING ERROR

CONFIG FAILED

I increase the MAX_RETRIES_FOR_PLL to 60 as well and still error exit.
I need you suggestion to fixe this issue. I have uploaded code as well

thanks
upeksha

Hello,

Qorvo is not providing official support for Makerfabs module but perhaps our community may be able to help. It looks like attachment of the code did not get attached. It will also be good to share the version of the driver that you are using.