Using .meas I can indeed output a list of text showing the voltage values for some selected nodes, but this is only a workaround.
In the Qspice Documentation I cannot find any time parameter for the .op analysis.
The .dc analysis is to sweep a dc value of a voltage/current source, which is not really the issue in my case.
Actually, it would be helpful to have a time parameter for .op in order to reflect all the voltage/current pairs, not at t=0s, but at t=Ns with N the time value in seconds, after the simulation was started.
This would be to show the various final values in the circuit, at the moment where the switch-on operation has stabilized and all transients have passed.
Using the .plot graphs, on the other hand, both transients and stabilized values are perfectly viewable, to show what happens at various nodes during the interval between t=0 and t=N
It would just be a nice added feature if the final values for t=N could all be reflected at the nodes in the circuit ?