Hi everyone,
I would like to share with you a development that I have made recently. It is a firmware developed with ChibiOS that allows access to all radio records in a simpler way and also includes functionalities to send messages with the 802.15.4 standard and the calculation of distances between nodes. It still has a lot of work to do, but at this point it is in version 0.1 and I think it might interest someone.
If I see that the idea generates interest, I have in mind to develop an API that works in conjunction with this firmware to design an application that allows to automatically calculate distances and angles between the different nodes of a network and return these values through UART. It would also allow adding and removing nodes automatically as well as calibrating the antennas.
I hope it helps you 
Here is the link of the repository.
Have a nice day.
Álvaro.