Here is a minor new feature: in Qspice, if you need to view .param values, you can add .option listparam to display all parameter values in the Output Window. However, if your design includes subcircuits, it also outputs every parameter within those subcircuits, resulting in a very long list.
To address this, Mike updated Qspice so that LISTPARAM now accepts an optional quoted pattern string to filter and limit the listed parameters.
For example,
.options listparam "*": list only those at global scope.options listparam "*?*": list those at global or one layer down
Since only the help file is updated and not mentioned in the revision notes, I think it is better to leave a note here.