hi,
i want to acheive multi tag and multi intiator within minimum amount of time. i tried some logic for single tag and two anchor, it works perfectly but i need to work with atleast of 10 anchors and multiples of tags, the point is, if i am work with the same logic which i used in my project definitely i got the timing issues, so kindly help me to sort out this issues , assist me with some algorithm for my neeed…
my logic mentioned here::
i programmed two devices as a anchors and one as a tag
if the 1st anchor send the request to the tag , at the same time the second anchor will receive the same message from 1st anchor, after that i disable the transmit mode in 1st anchor the receive the tag response, on otherhand the 2nd tag enable the transmit mode and send the request message to tag and 1st anchor, 1st anchor enable the transmission and wait until the tag give the resposne to the anchor 2. this process continues … i still confuse to sort out… kindly help me to acheive…
Thanks in advance