Hi. Like many others in the forum, I cannot achieve anywhere near the ~12 uA as suggested on the datasheet. I believe I have configured my module in a manner that should consume less current than any other mode, but I am still measuring ~10 mA when sleeping. I’ve attached a picture of my configure_module() function. Keep in mind that these are not the only settings I have tried. I have tried just about every combination there is to try and achieve the 12 uA without success. Any suggestions are much appreciated. Thanks in advance! - Cormac