I use MDEK1001 device for my internship project. I cannot connect any tag or anchor with my pc using serial port. I use Ubuntu 20.04 operation system and also try minicom and putty which is serial connection application. I can see this device in PC but cannot connect as an series. Minicom’s scene stay like given code in below, and if i want to write anything it writting as a @ symbol. I cannot see any letter or number or ex…
`
Welcome to minicom 2.7.1
OPTIONS: I18n
Compiled on Dec 23 2019, 02:06:26.
Port /dev/ttyACM0, 10:12:56
I tried to download PANS firmware but not finding any website for download. So consequently i have not PANS firmware. Do you think problem is this? If you can find, please give me link for download PANS firmware.
When you download the files, head to DWM1001/Product_and_Design_Documents/DWM1001-Firmware-User-Guide.pdf (This pdf is a guide on how to download the software you need to add the firmware to the devices)
The firmware can be found in DWM1001/Factory_Firmware_Image
You basically use the hex file as instructed in the user guide and you should be set
And if you have an android, you can also download the APK from the first link.
Thanks for your attention firstly. I apply this steps but nothing is change. I tried to upload .hex file using JFlashLite app on tag. I alwayys get an error as > Conecting to J-Link… > ERROR: Cannot connect to J-Link. > Done.
Are you running it with these exact parameters? The only issues I can think of is that the device is not connected, or you’re not using the correct parameters.
Hi @youssef@duygud
I see that the docs it too long to read . The @ is actually the readable part of an error packet which is returning the binary API interface. If you want to enter into the shell mode you need to hit enter twice (hit it twice fast).