Is it possible to configure the Preamble length the NTM_1 and NTM_2 (noise threshold multipliers) for the MDEK1001?
Configuration settings for these are stated in the “Part 2 NLOS Operation and Optimizations” application note which I intend to use in order to improve the NLOS performance.
Unfortunately, I do not have access to the PANS library and I couldn’t find a way to configure the MDEK1001 modules for NLOS conditions by using the API.
Is there any way to apply the settings to the MDEK1001 modules?
Any thoughts on this are appreciated.