I have a technical drawing as the example below. But the UWB tracking should only be available in two rooms, I have the actual measurement of the two rooms (displayed in red) in meters calculated and want to place the anchors as show.
I am aware that I need to use two gateways as the rooms are on different floors and are not in radio reach of each other
I want to be able that the system detects if a Tag is located in either room A or B and of course it’s position in the room.
The measurements taken should be received via MQTT within the application I have written and display the TAG accordingly
At the moment I have create one 1 network and as I understood the two gateways need to be in the same network anyway.
I have the following questions, how to configure the system.
-
How does the system determine in which “subnetwork/room” a tag is located as when I look at the mqtt message, there is no information of which anchor is detecting the tag or which anchor is detected by the tag. how can i get this information?
“dwm/node/858b/uplink/location b'{"position" {"x":0.78748477,"y":-.297379,"z":2.596518,"quality":98},"superFrameNumber":674}'”
-
when I place the anchor I assume each room needs it’s own initiator, since the two rooms don’t reach each other via radio signal. Can I configure the initiator’s position as 0.0 in each room and than place the other anchors in the same room base on the distance I have calculated ?
thanks you.