Hi all,
I’m trying to set a RTLS using MDEK1001/DWM1001 as anchors and DW1000+arduino as tags. I know it looks like a very particular design but I kind of have the need for it. The arduino library I’m using is thotro’s arduino-dw1000 (https://github.com/thotro/arduino-dw1000) and it is working perfectly when I use DW1000 as tags AND anchors. The problem comes when I want to make them work with the MDEK1001/DWM1001 devices: I set the anchors with MDEK1001 and tags with arduino-dw1000, but they can’t communicate. Of course I configure them with the same network ID. Do any of you know what may be causing trouble? Or maybe another way of making this work like different libraries or something like that?
Also, I’ve been wondering if this could be a protocol disagree, as if the creator of the arduino-dw1000 library had designed his own one. How could I sniff the packets between MDEK1001/DWM1001s interchange in order to see if they match the messages protocol going on with arduino-dw1000?
Thank all in advance, would really appreciate your help.
Greetings