We have considerable experience in industrial and warehouse UWB systems.  We offer consulting services to help match your expectations with what the technology can do, and just as importantly what it can’t do, and to guide how to best achieve your results.  A little bit of expertise applied at the beginning can make a big difference in the outcome.
I’d be happy to arrange a call with you to discuss your application and provide preliminary feedback on the feasibility.
We offer some generic devices, particularly the DWETH anchors and DWTAG tags.  Our products can be seen here:
https://www.ciholas.com/shop/
They may not be perfectly suited to your needs out of the box, but we also offer customization services to develop something that works exactly as you need.  Most commonly, we develop custom tags as that is the part most in need of being tailored to the task.  We design a new custom tag about every month or so lately, so this is a common exercise.  Our system can also work with customer designed tags that are using DWM1001 modules.
The DWETH anchors have been used in a wide variety of places, from museums to warehouses.  One of the key features is chainable power and Ethernet which reduces wiring by 90% over home run PoE.  Up to 12 DWETH101 can be powered on a single chain.  This greatly reduces one of the major issues with wired anchors which ultimately are the right solution in most working applications.
Our software produces output in IP packets containing tag ID, time, XYZ location, and location quality.  We can also output sensor data such as accel, gyro, mag, and orientation.  We can support large numbers of tags operating at high rate.
1000 m^2 area is not a problem, we can build much larger systems.
What is your target update rate?  Accuracy?  Battery life?
How effective the system will be is determined in large part by the conditions of use, namely where/how the tag is mounted to the pallet, how high the ceilings are in the active space, and the number and nature of the obstructions between tag and anchors.
Mike Ciholas, President, Ciholas, Inc
3700 Bell Road, Newburgh, IN 47630 USA
mikec@ciholas.com
+1 812 962 9408