Les no output on the bridge node

Hi,

I have set up a small network consisting of 4 anchors, 1 listener, and 1 tag using DWM1001 dev-boards. the listener is connected to my laptop through UART using PUTTY.

The problem is: I suppose that when I type ‘les’ on the bridge (listener) node’s interface, I should be able to get the tag’s location. But right now, when I type ‘les’, nothing happens. Below is a screenshot grabed from my bridge node. Can someone tell me why I’m getting nothing from the ‘les’ command? Thank you!

1

Hi,

The Bridge mode is something else then the Listener. You need to put the device to UWB Passive so it would be in Listener mode. E.g. using

acas 0 0 0 1 0 1 0
reset

Cheers,
TDK

Hi,

Thank you for your reply! Here is a snapshot from the listener UART window. So I entered the commands and the node should be configured as a passive anchor. However, there’s still no output when i enter ‘les’, ‘lec’, or ‘lep’. Do you know what could be wrong??

Best

Hi Hobian,

The listneer PanId is not set. You can set it using the nis command.

Also, how far is the tag from the listener ?

Thanks
Yves

Hi,

the Listeners is connected, so the Tag is probably out of range of the Listener or is not present.

Cheers,
TDK