Large Scale Network (Initialy Tag follow up over 2 network PANID change)

I do understand for the change of network.
What I did understood is the fact that with one initiator we should have only 30 Anchors.
What I do understand from your answer is that we can extend the network further. (Let’s say with a grid like in Figure 12 of the system overview).
I imagine that when I do this I need more initiators in the grid to synchronize the network on the right of the figure 12.
What is still unclear is how the border of the two regions builds.
It is said : “Fully scalable network: Anchor seats and TWR slots can be reused is sufficient space between nodes”

Does this means that we need to have a free space between the two zones so that anchor on the left don’t hear anchor on the right?

If so this means that in between the tag localisation is not very good/redundant.

Is it possible to have a handover between the two zones?

Could you please explain.
Thanks in advance.