Hello,
I used several anchors that are configured with a different height. Moreover, I have one listener that is connected to the computer and one active tag that is moving around and has almost a constant height (~1.70). I wonder why in my output of lec my tag has varying heights that are much to high (e.g. 2.10 or 1.95).
POS,0,C704,-0.51,6.36,2.10,97,x06
POS,0,C704,-0.39,6.31,2.10,99,x06
POS,0,C704,-0.17,6.28,1.95,98,x06
POS,0,C704,-0.00,6.29,2.07,96,x06
POS,0,C704,0.24,6.28,1.96,95,x06
POS,0,C704,0.27,6.29,2.19,93,x06
Could it be possible that you cannot have anchors which have not the same height? Do I have to many anchors (there are 7 anchors and one of them is 5 meters higher than the others that only vary in ~1m)?
Thanks in advance!
Best regards,
Blubbus