Is there a guide of how to perform firmware update using the “dw_updater”?
This problem has been resolved.
This problem was due to the virtual adapter.
Hi okhyun,
i have the same problem with you, the dw_updater.exe cannot find the Anchor. Can you please explain me how you have solved it.
Thank you in advance
Just a small guide:
-Install AC6 Eclipse Environment the process is described in the TTK1000 Anchor Source Code Guide
-Compile the anchors source Code using the “fw2” profile (TDoA RTLS application)
-Properties->C/C++ Build
-Install SolarWinds TFTP Server (or any other similar software)
-Copy the “Release/File anchor_F429.bin” (new firmware) on the TFTP Server root folder
RELEASE
SOLARWIND TFTP
-Configure your ethernet IP in the same range as the anchors
-Connect the host PC to the network
-Connect the already programmed (old firmware) anchors to the network
-Run the DW Updater as administrator
-Reset the anchors (Turn PoE Power off, turn off Poe Switch, dissconect ethernet cable, send reset
command trough controller, etc.)
-You will start to see the devices in the DW Updater
-double click in the desired anchors to be upgraded
-Close the DW updater one time all the selected anchors disappear from the awaiting list
-In SolarWinds you are able to detect if the anchors establish a download connection with the TFTP
Server
-All the Anchors physical settings should remain equal (IP, Netmask, Gateway, UseStatic, etc.)
-That’s all Folks