Is the 3.3V pin on J10 of DWM1001-dev working?

Hello,

I need to power the DWM1001-dev via its 3.3V pin, but seems like the 3.3V pin on J10 is not connected with the 3.3V of the DWM1001, from the schematic below there is a cross on the 3.3V PIN does that means it’s obsoleted?
dwm1001-dev%20J10
If so, how do I power it with 3.3V power source? (I have another 3.3V device need to power as well hence I don’t want to use the 5V pin)

The J10 PIN1 (+3V3) is not connected as shown on the schematic snapshot.
Maybe the best place to connect your 3V3 is at R23, remove it and connect on the right side.