Previously, in the Arduino UNO environment, data was not verified unless IRQ and RST pins were assigned.
Do I have to assign IRQ pins and RST to GPIO when I proceed with development with the development board with DWM 1000 or DWM 3000?
Then, I wonder if I should allocate RST and IRQ to any GPIO without restriction when allocating them to GPIO.
In addition, I heard that when positioning technology using anchor and tag, with the DWM 3000 model, a single anchor is sufficient must not two anchor, unlike the DWM 1000. Is that correct information?