Interoperability of QM33120WDK2 and QM35825K-05 dev kits?

Does anyone have experience with mixing parts from these two dev kits and then using them for RTLS demos?
–In particular using one of the quad antenna QM358 MultiOV boards as anchor and one or more of the LC14 boards as tags?
Does the Qorvo SDK support support both ends of this configuration (and the host app.at the anchor end)?

Hi @mikew67,

For the RTLS (TDoA) demos, QM33120WDK2 is running the software from @leapslabs which is proprietary whereas QM35825DK-05 is focused on FiRa.

The hardware is compatible but the software is not compatible out of the box.