I’m running a very simple noise simulation with an RROPAMP amplifier. It seems like the IN noise parameter is only calculated on the inverting input, but not on the non-inverting input, making the total output noise seem far too low.
I’d like to add the simulation file, but I can’t (new user).
I’m seeing only 40nV/sqrt(Hz); which is 10p * 4k. The non-inverting input should add another 10p * 1k * 5 = 50 nV/sqrt(Hz)