Ideal UWB product for Raspberry PI 4

Hi. I am looking for suggestions on which UWB product of yours I can use with Raspberry Pi 4. I am planning to use UWB for local positioning system for UAV in indoor environment for my project. Ideally would like to connect the UWB to a few pins on Raspberry Pi 4 (as I am attaching few other sensors on raspberry pi) and get the position of tag on-board wrt anchors. Is this possible to do? If so where do I look for setting this up? Can someone please help me with this and help me with the process. I am new so any help is much appreciated.

I made a direct connection of the DW1000 to RPi4b.

  1. Connect SPI interface of the DW1000 to a SPI of the RPI4, and connect INT pin too to one of the GPIOs of the RPI4;
    2)Create and compile dtbo file for the RPI4, where this connection is described, so RPiOS can work with the pins as needed;
  2. Turn on the SPI interface on an RPi4;
  3. There are several Linux drivers on the github. Choose one and compile for your version of the kernel. Sometimes small modifications should be done due to version differences(deprecations mostly)
  4. You have an interface in the system with which you can work.