I have developed UWB boards using the DWM3000. I have the ESP32 S3 interfaced to the DWM3000. I have both anchor and tag working nicely. I want to interface with the Apple tag but have been told by Claude AI the onlr libraries and code from Qorvo is the DWM3001C. That part uses the nRF5233. The Apple compatible code was written for the nRF5233. The UWB Part or each is the DW3110. How can I get library source code that interfaces with Apple that I can feed into Claude and he converts to ESP32? To see mu boards go to www.starcomeng.com.
The DW3 1.1.1 sdk has the interface code. it runs on 52833, 52840, and another I can’t remember.
But the Fira libs are binary only.
I’ve used the Apple interface design to make an Android compatible version
And that runs the same place the Qorvo QANI (apple nearby) build works