How to use multiple(more tha 9 anchor) setup using DWM3001CDK?

Peer limit when using initf -multi via CLI

Hello,

I am using the CLI with the reference firmware and observing a peer limit when configuring multi-node ranging.

Command

initf -multi -addr=0 -paddr=[0,2,3,4,6,7,8,9,10]

Issue

When the number of peer addresses exceeds 8, the command fails.
The CLI (Minicom) reports:

Command

KO
Number of peers exceeds the max: (8)

Question

Is this 8-peer limit an intentional design constraint of the reference firmware, or is there a supported way (configuration or firmware modification) to scale beyond 8 peers when using the CLI?

Any guidance or recommended approach would be appreciated.

Best regards,
Lakshya

Hi Lakshyaa1,

Yes, the number of responders is limited up to 8 devices following the FiRa UCI spec. This is described in Application configuration paramaters. Unfortunately, this is fixed in the fw and cannot exceed the limit of 8 peer devices.

Cheers,
LC_Qorvo