How to use DWM3001CDK with Apple NI

I have purchased the DWM3001CDK development kit. I have also downloaded the software download. I have flashed the file “nRF52840DK-QANI-FreeRTOS.hex” to the board using JFlashLite. The board does not show up on the Qorvo Nearby Interaction app on my iPhone 13 Pro (it is stuck on “Scanning for accessories”). Could anyone help me out here?

1 Like

Hi Ashley3120,
Since you have purchased the DWM3001CDK dev kit, I recommend that you flash it with the image labelled “DWM3001CDK-QANI-FreeRTOS.hex” first and then try to connect to it with the Qorvo Nearby Interaction app afterwards.

Hope that helps!

Best regards,
-Quan

Hi Ashley3120,
A colleague pointed out that my original reply may not have been clear. In that case, please note that based on your original message, you have used the incorrect binary to load onto your DWM3001C.

Please use the filename “DWM3001CDK-QANI-FreeRTOS.hex” to load onto your DWM3001C device. We have 3 platforms that the SDK supports, please use the correct one for your platform.

best regards,
-Quan

Thank you Quan. I did as you suggested and it works now.

Can someone help me?
Windows test: Qorvo UWB Explorer succeeded.
Apple test: Cannot find the device; BLE seems to be not broadcasting.
iPhone version: iPhone 13, iOS 18.5.
Testing with the DWM3001CDK_C2 SDK to burn the following two versions failed:
DWM3001CDK-QANI-FreeRTOS_full_QNI_3_0_0.hex
DWM3001CDK-QANI-FreeRTOS.hex

FIXED
https://devzone.nordicsemi.com/f/nordic-q-a/112427/nrf52833-report-error-peer_manager_pds-could-not-initialize-flash-storage-fds_init-returned-0x860a?ReplyFilter=Answers&ReplySortBy=Answers&ReplySortOrder=Descending
flashing DWM3001CDK-QANI-FreeRTOS_full_QNI_3_0_0.hex, keep the DWM3001CDK plugged to J9 and open the J-Link RTT Viewer app.
The message below shows the problem.
00> peer_manager_pds: Could not initialize flash storage. fds_init() returned 0x860A.
00> peer_manager: pm_init failed because pds_init() returned NRF_ERROR_STORAGE_FULL.
00> app: Fatal error