Hi,
How to show on y-axis unit in J(Joule)?
I see that if I put 100uF in the plot I received an error:

I want to see something like this:

Hi,
How to show on y-axis unit in J(Joule)?
I see that if I put 100uF in the plot I received an error:

I want to see something like this:

Capacitor energy is 1/2*C*V^2, and it appears that the 1/2 factor is missing.
To display the energy in Joule, you can modify the formula to 1/2*100µ*V(N36,GND)^2/1V^2*1J
Ok, i will try this by adding 1J at final in formula in plot. Thank You.
No worry, I am aware about this that energy of capacitor has also a factor of 1/2 in front. This time and this post I did not want to be about energy of capacitor formula, but more about how to show units J in plot.
Another question: do you know if it is possible to change from nJ to 0uJ? Like 500nJ=0.5uJ.
I tried by changing the axis values:
Hm, I found that this ca be done like this, but is it correct?
I need to multiply also with 10^2:
1/2*1*I(L7)^2/1A^2*1J*10^2
If you need the scale to display in u instead of n for 500n, what you can do is to change Axis Setup. If you multiple by 10^2, you actually change the value by multiple it by 100.
Here is the example, if you can manage to show from nJ to uJ y-axis in the plot in order to show 0.5uJ not the equivalent 500nJ:
plot nJ to uJ.qsch (5.9 KB)

0.5uJ = 500nJ … what the problem?
Or you are saying you want the red cursor give 0.5uJ in uJ scaling?
Not sure why, sometime I can easily confuse with the questions.
Yes, two things:
If it is the cursor, I don’t know of a way to change it. It appears to be fully automatic.
Ok then, understood.