Hello
I want to run the DWM3001C API code (example code “ex_06a_ss_twr_initiator and ex06b_ss_twr_responder” from https://www.qorvo.com/products/d/da007992) on DWM3001CDK board.
However the DWM3001C API source code only support nRF52840-DK and STM_Nucleo_F429 board. While DWM3001CDK is nRF52833.
Is there easy way to run the code on DWM3001CDK? or should I migrate the code from nRF52840 to nRF52833?
Thanks
Hi @jiwoong ,
Yes right, you need to migrate the from nRF52840 to 833.
Check my comment in this topic Getting started with DWM3001CDKE - #6 by illysky.
I hope this will help you !
Hi Team,
I am new to UWB technology and have started working with your DWM3001C module for an RTLS application. I would like to understand the development flexibility and firmware capabilities of this module. Please help clarify the points below:
- Does the DWM3001C module have a built-in CPU/MCU on which users can develop and run their own application on top of your provided stack?
- Is it feasible to load custom firmware onto this module?
- If yes, what level of user control is available over the firmware?
- What tools and development resources are required to start development?
- SDKs, IDEs, compilers
- Debug/programming tools
- Reference documentation or example projects
- For RTLS use cases:
- Can the same DWM3001C module be configured and used as both Tag firmware and Anchor firmware?
- Is this role purely firmware-based?
- Does the module support complete user control for developing custom applications?
- In the future, we plan to interface additional sensors with this module. Please confirm whether this is supported and any limitations we should be aware of.
Kindly share the relevant documentation, application notes, and recommended steps to get started with development.
Regards,
Kumar
Hi @francis.kumar
I would recommend you to start with QM33120WDK2 - Qorvo demokit. Which comes with preloaded demo LEAPS RTLS firmware.
Regarding your questions - see my answers below:
- Does the DWM3001C module have a built-in CPU/MCU on which users can develop and run their own application on top of your provided stack?
Yes it have onboard CPU - nRF52833. Qorvo is only providing basic examples.
- Is it feasible to load custom firmware onto this module?
- If yes, what level of user control is available over the firmware?
For sure, you can do it. You can develop your own solution or use some 3rd party binary stack.
- What tools and development resources are required to start development?
- SDKs, IDEs, compilers
- Debug/programming tools
- Reference documentation or example projects
The DWM3001CDK and QM33120WDK2 dev kit comes with onboard debugger tools. Then you can use any IDE you like. Segger is a good one or you can use opensource solution based on VS Codium or Eclipse based one.
- For RTLS use cases:
- Can the same DWM3001C module be configured and used as both Tag firmware and Anchor firmware?
- Is this role purely firmware-based?
Qorvo does not provide any RTLS firmware for DWM3001C modules. You need to develop one by your self or use 3rd party one.
- Does the module support complete user control for developing custom applications?
- In the future, we plan to interface additional sensors with this module. Please confirm whether this is supported and any limitations we should be aware of.
As the module contains no firmware then you can develop anything you want - you have full access to the MCU.
Cheers
JK