I am trying to get positions of multiple tags at the same time using DWM1001.
I can get location of the tag connected to my PC by les command but I can’t get the others.
What settings should I make to get all the tags?
And is there any way I can save the log info in the serial port terminal to a file?
If you are entering the command les
when connected to that particular tag via PC, it will only give you the position of that tag.
If you need position of multiple tag, make one module as listener
and connect that to the PC, while other tags are on, and enter les
command. You will get the position data of all the tags,
‘les’ command doesn’t provide the distance when a anchor is configured in 'passive mode.
In only returns the position