Hi
I have 4 anchors and 1 tag. All of them are working fine on the android app and is showing the location of tag. They are showing FW2 as operating firmware.
I also have setup one anchor as bridge mode using nis and nmb commands. I have mounted it on top of raspberry pi. I can access it using UART in pi. When I run si command to get the system information I can see its a bridge node by looking at the following line:
[000018.580 INF] opt: AN [color=#ffcc33]BRIDGE[/color] LEDS BPC UWB0 I2C SPI UART
But when I run command “la” to get the list of anchors it doesn’t show any anchors while all of them are with same network id.
[color=#333333]dwm> la
[/color]
[color=#333333][000008.900 INF] AN: cnt=0 seq=xFF[/color]
[color=#333333][000008.900 INF][/color]
I think the location engine in the tag is enabled as I can see it in tag info in the Android app but didn’t found any option to check location engine for anchors.
How can I resolve this issue? How can I get the list of connected tags/anchors and then get the location of tags in Raspberry pi.?
Thanks