How to generate delay times between two signals?

Hello,

Is it possible to generate these two signals having 2 switches and 1 pulse signal that is driving the 2 switches? The problem is in how to make td1 and td2 (for example td1 = 10ns, td2 = 10ns)…
PULSE(0 10 0 1n 1n 1m 2m)
.model MYSW SW(Ron=0.1m Roff=100Meg Vt=0.005)

1 Like

You want to create a symmetrical signal between S1 and S2, or S1 duty must be 50% (or certain value) and S2 is conjugate but with different deadtime td1 and td2?

Here is for symmetrical signal

1 Like

I know that this thing can be done with two signal pulses. The question was how to do this with 1 signal pulse only.

Not the only way to do it (but probably the most fun way) you can put in a delay filter and comparator.

or you can do it the SPICE voltage source way:

Also you can now use C++ and verilog, but someone else will need to demonstrate that.

Only a single source S1 in your system?
Imagine that, when S1 turn off, with a delay for S2 to turn on is easy. But how S2 know when to turn OFF if you only have one source in your system. You must have some sort of clk signal to help.

I found the way how to do this:
@KSKelvin can you translate this schematic in QSPICE?


This is how this circuit can be implemented in Qspice. Basically, this is symmetical and the trick is replicate master signal itself with an inverter (or in your example, B-source -V(a)+10)

I don’t like the idea of using -V(a)+10 as this is not something you will practically implement.
Therefore, I just simply use an inverter and change a bit of this logic implementation. Practical delay implementation is already mentioned by @jay314159265.

Deadtime for Symmetical Signal - Master Source Only.qsch (7.0 KB)

1 Like

And how to change the amplitude of V(gate1) and V(gate2) to be 10V for high and 0V for low? right now is 1V for high and 0V for low

Here you go.

Deadtime for Symmetical Signal - Master Source Only - Vdd.qsch (7.1 KB)

This is practical circuit implementation with R-C delay.
Deadtime for Symmetical Signal - Master Source Only - Practical Delay.qsch (8.1 KB)

2 Likes

For V(gate1) or V(gate2) from 1V peak to 10V peak, another way is just to use a B-source, with formula likes V=10*V(gate1).

I have done this for LTspice. Please, check out this video.
It can be done in the same way for Qspice.

2 Likes

You can also use the idt() function to create a time to voltage converter with either behavioral voltage or current sources as is done in the LTspiceControlLibrary for their ComplementaryBufferWithDeadtime. Works well.

GitHub - kanedahiroshi/LTspiceControlLibrary: A LTspice library for designing controller by drwaing control block diagram

Here is a breakdown

ComplementaryBufferwithDeadtime.qsch (15.0 KB)

1 Like

The programmable deadtime driver from @marcos.uniovi in previous reply is replicated in Qspice. This is the embedded symbol and demo schematic. Deadtime is controlled by an attribute tau.
+ProgDeadtime.qsym (1.6 KB)
Parent.+ProgDeadtime.qsch (4.9 KB)

Below is a full schematic of this driver as according Prof. Marcos youtube video. I made slightly modification by including a buffer at input signal to ensure voltage in next stage (with RC delay elements) must be 1V/0V to prevent input signal amplitude affect deadtime calculation. In addition, the logic threshold of ¥1 and ¥2 are set to e^-1 or 1-e^-1, which is also to ensure deadtime match RC time constant. Hope that I don’t make any mistake in this LTspice replication work.
Programmable Deadtime Driver.qsch (27.3 KB)

4 Likes

This is great. Thank you very much for this effort.

1 Like

Hi,

Thanks Professor Marcos and KSKelvin for this block.

I’m using it and found a weird behaviour where repeating the instance caused both instances to work differently.

I’m using two dead time generators, for one of them, the input is followed by the high side gate while in the other one the input is followed by the low side gate. In the picture below, the top 4 traces are one dead time generator and the bottom 4 are the other one. The issue is gate 1 follows a2, but gate 3 is the oposite than b2.


Find attached the sch.
dummy_Rectifier.qsch (17.7 KB)

Any Ideas why this might be happening? (The converter is an active full bridge rectifier)

Regards

This deadtime circuit is @marcos.uniovi design. The best answer may come from Prof. Alonso.
From the waveform, what you can observe is that, you have input pulse with pulse width less than deadtime. This will mess the toggle sequence in this circuit with D flip-flop and therefore, you may get an output opposite to input over time.

I have another deadtime logic that don’t need a flip-flop, you can check if can handle this situation. But it is logic output, and you have to add E-source to buffer the logic output to drive the FET.
Gate-DeadTime.qsym (1.8 KB)

2 Likes

Worked like a charm! Thanks