I’m asking if someone knows… How many Anchors and Tags can be active at the same time?
Hi Daniel,
Please have a look at the system performance overview and also on other thread on the forum, this was discussed several time.
There is no straight forward answer but basically, the tag capacity is 150 Hz (so for example 10 tags at 10Hz) and 30 anchors seat. But both anchors seats and tag slot can be reused if the network is correctly deployed (which basically means with a network deployed over a large area, you could have 60 anchors and twice 15*10Hz tag)
Thanks
Yves