I am trying to simulate the circuit inside of a 555 timer. I would like the post-process window to show the eventual frequency of V(OUT) once the waveform settles. Not having any success. The directives I used are listed below.
.tran 100m
.plot V(TRIG) // Vc1 voltage at C1
.plot V(Q)
.plot V(OUT) // Q not signal
.meas frequency V(OUT) at T=50m to T=100m
Update: Forgot to show what displays in pre-processor window. V(OUT) plots fine and the frequency should be about 100Hz. But what the pre-processor window does not show this. What it does show is below:
.meas freq v(out):
4.81838 0.1