Hardware for 1 anchor 4 tags setup, DWM3000EVB?

Hello!
I am very new to Qorvo/decawave and I am evaluating UWB for following scenario:
1 anchor that should be able to measure distance for 4 tags within a range of 10 meters.
Should a set of 5 DWM3000EVB mounted on 5 nrf52840 development kits be enough for such a setup or do I need anything else? Moreover, is there any sample code for such a case where 1 anchor is able to calculate distance of 4 tags in proximity with a time resolution of 10ms (distance update every 10ms)?

Please also recommend hardware/EVK to be used as anchor to get 2 dimentional distance data, perhaps a module with multiple antennas?