Work on demo version of Qorvo nearby Interaction firmware.
. = ASSERT(stack_process_start == stack_process_end || (stack_process_end - RAM_segment_start) <= RAM_segment_size , “error: .stack_process is too large to fit in RAM memory segment”);
I only added a few lies to change the tx_power.
And built a relase version so it should take less memory right?
Any clues?
added these lines to main_uwb_main.c
16: include “deca_device_api.h”
18:int err;
19: uint32_t adjtxpower;
20: uint16_t appliedboost;
185: err = dwt_adjust_tx_power(0, 0xfefefefe, 9, &adjtxpower, &appliedboost);
try to declare return variables as pointer (*) but got compiler error say &adjtxpower was double pointer **
C++ is not me first language.