Impedance matching is often the bridge between selecting an RF device and integrating that device into a larger design.
Within the broader design journey:
System Requirements → Component Selection → Impedance Matching → Hardware Validation
Qorvo MatchCalc™ focuses on the impedance matching step. It is a downloadable RF/microwave matching calculator designed to help engineers develop and tune matching networks using S1P or S2P data.
Where MatchCalc fits
A typical use case starts after you’ve identified a candidate RF device and have its measured or simulated S-parameter data.
From there, MatchCalc can help you:
- Import S1P or S2P files
- View impedance, return loss and insertion loss/gain
- Visualize the response on a Smith chart
- Add and tune matching components
- Use markers and snapshots to compare matching attempts
- Save matched S-parameter results or generate a match report
MatchCalc is a focused impedance-matching tool.
Getting started with MatchCalc
Start from the Qorvo MatchCalc page and download the Windows application.
Once installed:
- Obtain the S1P or S2P data for the device or network you want to match.
- Load the file into MatchCalc.
- Select the plots and frequency range you want to monitor.
- Capture a snapshot of the starting response.
- Add the desired matching components.
- Tune component values while monitoring impedance, return loss, gain and Smith-chart response.
- Save the resulting design or matched S-parameter data.
Available Qorvo device data can be found through Qorvo Design Files.
A practical first use case
Suppose you’ve selected an RF device and downloaded its S2P file.
Load the file into MatchCalc and begin by displaying the input impedance and return loss over the operating band.
Take a Snapshot of the original response, add matching components, and tune the component values while comparing the new response with the original.
Once you’ve reached a useful match, the matching topology, component values or matched S-parameter data can move forward with the rest of the design.
How to Use Snapshot and Markers
Where to go next
Once the matching network is developed, the design can move forward into broader modeling and evaluation.
Related resources include QSPICE® for power simulation, the QSPICE Technical Forum here on the Qorvo Tech Forum, and the broader Qorvo Design Tools Library.
How are you using MatchCalc?
If you’ve used MatchCalc, what does your typical matching workflow look like?
Are you starting from measured or simulated S-parameters? Which plots or features do you find most useful when tuning a match?
Share your examples, questions or tips below.