Dear admins
Does Qspice have an equivalent LTSpice command to use an external frequency table like:
.subckt Rs 1 2
R1 1 10 0.01
V1 10 11 0
B1 11 2 V=I(V1) MAG FREQ=
.include T50-6.txt
.ends
The solution given by KSKelvin in the “FREQ function ad LTSpice equivaslent” topic requires the same number of sweeps as table lines, which implies a long calculation time.
Thanks in advance.
Regards.
JJ64