However, the file referred to in the DWM1001 Firmware API Guide: examples\ex1_TWR_2Hosts\tag\tag_cfg.c is missing, but there are two new examples. Is this done on purpose? If yes, maybe the firmware API guide should be updated accordingly?
Thank you for the reply. The file is mentioned in two guides available in the “Product_and_Design_Documents/” folder in the link mentioned above.
In the the “DWM1001 Firmware User Guide” in section “4.3.2.2: UART Generic mode example”
and section “4.4.2 SPI Example” on pages 25, 26 and 27.
It is also mentioned in the “DWM1001 Firmware API Guide-2.2”, called “DWM1001-API-Guide.pdf” in above mentioned folder, in section “5.2 Usage of the APIs” (Table 4).