I understand that firmware can be updated to Release 2 through the ardroid DRTLS manager.
I was wondering if there is any chance of downgrading the firmware back to the previous one through the app ? Instead of flashing the hex file for downgrading through J-Link.
Yes you could download the source code and recompile the android application with the hex file you want to use.
May I ask what you want to revert back to the previous release ?
Note that the new release only bring improvement from the previous one and that is only adds optional features. Anything you could do previously can still be done. Also, the old version does not respect regulation so should no be used for any commercial application.